picoScan100: Precise 2D LiDAR measurement data for localization of mobile robots
Von SICK AG
Ansichten
Von SICK AG
Diverse applications. One solution. picoScan100.
The picoScan100 2D LiDAR sensor offers tailor-made solutions for a wide range of applications. Whether used for the navigation of small autonomous mobile robots (AMRs), as a driver assistance system in industrial trucks, or in stationary applications, the picoScan100 can be easily integrated into almost any application – even in outdoor areas – thanks to its compact size.
AMRs use the measurement data of the picoScan100 to create a precise map of their environment. The current position and route of the AMR can be determined based on landmarks inside this map.
Reflector detection:
When the picoScan150 detects a reflector, this information is attached to the measured value and is available in the graphical user interface and in the data telegram. This makes it easier to differentiate between natural targets and reflectors.
Dynamic Sensing Profiles:
Adaptation of the measurement core parameters during operation and without rebooting for dynamic adjustment to the specific requirements in subtasks of the LiDAR sensor.
“One size fits all” sensor using AMRs as an example: From very accurate close range measuring tasks for fine positioning, e.g. docking at a charging station, right through to environment perception in navigation tasks with a large working range and fast response times for collision avoidance.