PeopleCounter is a SensorApp for people counting developed by SICK that enables the differentiation between people and objects within large areas of coverage. Based on the hardware of the MRS1000 3D LiDAR sensor, measurement data is generated as a point cloud. The integrated PeopleCounter app reliably identifies people based on their contours, thus ensuring only people are counted, while objects are blanked out. This process takes place anonymously and without recording any personal information.Thanks to the four scan layers of the sensor, the direction of movementof a person is clearly established. The people flow can be determined and the maximum capacity of people of a delimited zone can be monitored. To continuously keep track of the current capacity, the status of the counting is available via digital outputs. Thanks to the ability to combine resp. interconnectseveral sensors in an existing network, it is also possible to coverlarge areas with multiple entry and exit points, such as shopping centers, airports or trade fair buildings.Click here for more information:https://www.sick.com/PeopleCounter
- Tags
-