The individual process steps of a bottling system can be highly dynamically synchronized by means of rotary SICK A3M60 PROFIBUS encoders. Incremental encoder DFS60 detects the speed of the conveyor belt at which the filled bottles are led from the bottling system to the next process step.Alongside the mechanics, the drive and control system forms the core of such a system. To coordinate carousel movement and the filling process, the control needs information regarding speed and absolute position values. These can be identified by means of SICK incremental and absolute encoders.The latest SICK fieldbus-based encoders also come with extensive diagnostic functions tailored to the market, which guarantee our clients great added value. Remote maintenance, monitoring, high system availability, replacement security, flexibility and compactness are only a few attributes that distinguish SICK encoders
- Tags
-