multiScan100 – reliable 3D environment perception (rosbag replay)
Von SICK AG
Ansichten
Von SICK AG
With a large scanning range, fine angular resolution and high sensitivity, the multiScan100 3D LiDAR sensor is setting new standards in 3D environmental perception. It also reliably detects small and dark objects. The sensor delivers exact measurement data and features integrated processing of data that is transmitted to e.g. mobile robots.
The product family multiScan100 offers two hardware variants. One of the main difference is the field of view of 65° x 360° (multiScan136) and 42° x 360° (multiScan165). This rosbag recording shows both, the multiScan136 and multiScan165 in comparison.
You can download these rosbags yourself by clicking on the following link:
https://support.sick.com/sick-knowledgebase/article/?code=KA-09442
Click here for more information: https://www.sick.com/multiScan100