0:23 Description of the converter function block "UI8 to Boolean converter"1:00 Location of the "UI8 to Boolean converter" in the MOC logic editor1:36 The configuration of the "UI8 to Boolean converter"2:38 Simulation of the converting process from the "UI8 to Boolean converter"3:53 Routing signals from the MOC logic to the CPU logic6:10 Simulation of the converting process and the routing processPlease find more information find in the Flexi Soft Designer operating instruction or in the Drive Monitor FX3-MOC0 online help.
- Tags
-