With the MRS1000 multi-layer scanner, SICK has developed a 3D LiDAR sensor, also known as 3D laser scanner, which accurately and reliably detects and measures objects in good time and in multiple dimensions. By collecting large volumes of data on multiple scan layers and from different angles, it can detect and respond to objects on the floor as well as objects that are obstructing the path. The LiDAR sensor also features the innovative Ground Reference Evaluation (GRE) to constantly monitor the ground level and react on obstacles on the ground as well as missing ground.Click here for more information: https://www.sick.com/mrs1000
- Tags
-