To avoid thefts at points of sale, e.g. sales counters, shelves or display cabinets they can be secured by a combination of SICK sensors like RFID interrogators and antennas as well of laser detectors from SICK. If the authorized person leaves the point of sale, the sensor is activated. The area can be secured with a horizontal field (Secured Access Control). If an unauthorized person enters the point of sale, this will be reliably identified and an alarm is triggered. In addition, the point of sale can be secured via a vertical field (tamper theft protection), so it is not possible to grasp over the point of sale, without triggering an alarm. With this solution an early recognition is possible to improve the reaction and intervention time. Additionally a camera can be used for the verification and evidence.
- Tags
-