Laser detectors from SICK like the LMS531 reliably detect objects, even in adverse environmental con-ditions such as rain or snow. Main field of application is the detection of persons for the prevention of intrusion, outbreak, theft or vandalism. If an object is detected by the laser detector, the information can be given to a video management system and the object can be tracked by the camera efficiently. An alarm is triggered, the recordings of the cameras are displayed on monitors and the monitoring personnel can intervene.
- Tags
-