Increase safety and productivity of packaging machines with the modular Safeguard Detector safety system. The Safeguard Detector consists of the Flexi Soft safety controller and two MultiPulse photoelectric sensors. The Safeguard Detector securely detects whether a movable physical protective device is located at a previously defined position, e.g., the packaging material in the carton magazine of packaging machines. If there is sufficient material in the carton magazine, then it is not possible to reach into the hazardous area while the machine is running.
- Tags
-